How do I return a generator to automatic mode after service?

After servicing a Generac Next Generation 10–28 kW or Guardian 10–26 kW air-cooled standby generator, return the unit to AUTO mode to ensure it operates automatically during outages or exercise cycles. This includes engaging AUTO, confirming the green status light, reinstalling the 7.5 A fuse, setting the Main Line Circuit Breaker (MLCB) to ON, connecting a functional battery, completing the Install Wizard if prompted, and clearing the yellow maintenance reminder via the control panel or Mobile Link. Customers searching for terms such as “reset generator after service,” “generator auto mode,” “standby generator post-maintenance,” “generator not starting after maintenance,” “maintenance reminder,” or “maintenance warning” will find step-by-step guidance to ensure their generator is ready to run.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support