Can Multiple Transfer Switches Be Installed with a Single Generator?
When installing multiple transfer switches to be protected by a single generator, a relay may be necessary, and only one switch will provide the required T1 battery charge connection. Only wires 194/23/0 will be connected between the two transfer switches.