Can the Generator Be Mounted on a Roof, Platform, Wooden Deck, or Other Structure?

It must be placed in accordance with the requirements of NFPA 37, Section 4.1.3. The surface beneath the generator and beyond must be non-combustible to a minimum of 12". Contact the local Building Inspection Department or fire department to determine which noncombustible materials are approved for installation.

Loading
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support