Can the Startup Delay Time for a Home Standby Generator Be Adjusted?

The start-up delay is the brief pause before a standby generator begins supplying power after a utility outage. By default set to five seconds, it prevents unnecessary starts during short outages or voltage dips, reducing wear and ensuring smoother operation. This delay is adjustable by a certified technician between 2 seconds and 25 minutes, and differs from the built-in transfer delay of the automatic transfer switch.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support