What control panels do Generac's standby generators use?

RG series units 60 kW and smaller, or 100 kW and larger use evolution controllers located on the external housing of the generator. QT series units use a Nexus controller located behind a housing panel.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support