What's new about the Next Generation standby generator?

Next Generation (Next Gen) air-cooled home standby generators update the prior Guardian line with the PowerZone 200 controller, built-in cellular connectivity, EFIC engines with hydraulic lifters (no valve adjustments), a redesigned enclosure and rear connections, and models up to 28 kW. These changes reduce maintenance, simplify installation and service, and enable Mobile Link features such as Exercise Now, Exercise with Transfer, remote schedule edits, Smart Exercise, and oil-level visibility.

Title
What's new about the Next Generation standby generator?
URL Name
What-s-new-about-the-Next-Generation-standby-generator

Public Content
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support