How do I configure the fuel type on my air-cooled home standby generator?

Most Generac air-cooled home standby generators are factory-set for natural gas (NG) and many supported models can be configured for liquid propane (LP). Next Generation Series (10–28 kW): set fuel type in the Field Pro app during guided setup before first startup. Guardian Series (10–26 kW, 2017 to present): set the fuel selector knob for NG or LP and confirm Fuel Selection in the controller (Main Menu → Sub Menus → Edit → Fuel Selection). PowerPact 7.5 kW: convert by swapping fuel jets per the installation manual. Fuel flow and pressure must meet specs. Generac support cannot size gas lines/tanks/regulators but can provide BTU and fuel pressure (in. W.C.) guidance for your installer. Home standby units run on NG or LP only. Users searching for NG to LP conversion, propane conversion, change fuel type, set fuel selection, fuel selector knob, Guardian fuel conversion, Field Pro fuel setup, PowerPact fuel jet swap, and fuel pressure requirements.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support