What is the Generac Connectivity Cellular Accessory?This article provides an overview of the Generac Connectivity Cellular Accessory.Aug 31, 2026Knowledge
FieldsTitleWhat is the Generac Connectivity Cellular Accessory?URL NameWhat-is-the-G3-Connectivity-Cellular-AccessoryContentPublic ContentWhat is the Generac Connectivity Cellular Accessory? The Connectivity Cellular Accessory is Generac's next generation cellular connectivity device, designed to offer high signal reliability, robustness, and an easy installation process. This accessory is compatible with air-cooled and liquid-cooled generators operating on Cat-M1 technology and multiple carriers for U.S. and Canadian coverage. It maintains the same hardware, subscription price, and enrollment process as its predecessor. This device replaces the discontinued Wi-Fi/Ethernet and 4G LTE aftermarket accessories. For more information, see the Mobile Link Wi-Fi, cellular, and LTE device compatibility guide. Environment This article applies to the Generac Connectivity Cellular Accessory (model G0072150). Frequently asked questions What is the difference between the 4G LTE and Generac Connectivity Cellular device? The Generac Connectivity Cellular Accessory is the latest Generac cellular connectivity device with improved reliability and coverage. Key features Global coverageMulti-carrier extended coverageOperates on 4G and 5GHighly secureDesigned for IoT applicationsCat-M1Dual SIM card setup Does the Connectivity Cellular device support Wi-Fi? Yes. The Connectivity Cellular Accessory supports Wi-Fi as an optional backup connection. If cellular connectivity becomes unavailable, the device can switch to a configured Wi-Fi network. Cellular remains the primary connection whenever a cellular network is available. To set up Wi-Fi backup, the device firmware and Mobile Link app must be updated to the most current versions. See How do I set up Wi-Fi for my Connectivity Cellular Accessory? Can the Connectivity Cellular Accessory be set to use Wi-Fi only? No. The device is cellular-first and defaults to cellular connectivity whenever a cellular network is available. Wi-Fi serves only as an automatic backup. If cellular connectivity is unavailable, the device can switch to the configured Wi-Fi network. It cannot be configured to use Wi-Fi as the primary or sole connection method. Does the Generac Connectivity Cellular Accessory require a subscription? Mobile Link offers a Basic monitoring option as well as paid Premium subscription options. See What are the available Mobile Link subscription plans? Where can I purchase the Generac Connectivity Cellular Accessory? Contact a local Generac Independent Authorized Service Dealer (IASD) for availability. How can I find a Generac service dealer in my area? When ordering a Connectivity Cellular Accessory kit (G0072150) for a liquid cooled generator built before November 2024, an additional harness (part number A0005166075) is required for the following generators: RG02515RG03015RG04845RG06045RG08045RG10090RD03022 (also requires G0064780/0K2231)QT series (can also use G0064780/0K2231) The RG13090 and RG15090 require harness A0005792571 because of the generator size. RG13090RG15090 The RG03234, RG03824, RG04524, and RG06024 use harness A0005166075. The harness included with the Connectivity Cellular Accessory kit is A0005914366. This harness is not needed for the generators listed above and can be retained for use on other compatible liquid-cooled generators. What cellular carriers are available in the U.S. and Canada? U.S. carriers: Verizon, AT&T, US Cellular, T-Mobile, SprintCanadian carriers: Rogers Wireless, Bell, and Telus Note: For additional carrier options and to verify coverage in your area, contact a Generac Independent Authorized Service Dealer (IASD). Use the dealer locator to find a nearby dealer. Is the Generac Connectivity Cellular Accessory available outside the U.S. and Canada? No. The Generac Connectivity Cellular Accessory is currently available only in the U.S. and Canada. What type of warranty is offered with the Generac Connectivity Cellular Accessory? The accessory includes a one-year limited accessory warranty. Can I install it myself? Generac recommends working with a local Generac Independent Authorized Service Dealer (IASD) for installation. However, the device can be installed by an end user. See How to install the Mobile Link Generac Connectivity Cellular Accessory. See also How do I set up Wi-Fi for my Connectivity Cellular Accessory?
Was this article helpful?Choose a general reason-- Choose a general reason --FeedbackUpload FilesUpload FilesOr drop filesSubmit