Do you need to manually reset the clock in the unit for Daylight Savings?

Yes, the clock would require manual updating for Daylight Savings time changes, unless the customer is OK with the unit running one hour earlier/later, depending on the time change.

Title
Do you need to manually reset the clock in the unit for Daylight Savings?
URL Name
Do-you-need-to-manually-reset-the-clock-in-the-unit-for-Daylight-Savings

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support