Why is my home standby generator not exercising or exercising at the wrong time?

This article helps you fix a home standby generator that isn’t exercising or is exercising at the wrong time. It explains the most common cause—an active fault/alarm—and shows how to confirm the generator is in AUTO, clear alarms, and check the LED status. You’ll learn where to view and adjust exercise settings (Mobile Link for Next Generation/Power Zone 200, controller for Guardian/Evolution 1 & 2), how to verify 24-hour clock, date, and frequency (weekly/biweekly/monthly ≥10 kW), and why Smart Exercise might skip a run if the unit has run recently. It also covers checking the run log and correcting time after Daylight Saving Time or power/battery service. If settings are correct, there are no alarms (GREEN LED), and no exercise is recorded, the article directs you to a local Generac Independent Authorized Service Dealer (IASD) via the dealer locator.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support