How do I find out how many run hours are on my home standby generator?

This article explains what generator run hours are (total engine operating time) and how they differ from hours of protection (elapsed time since activation). It applies to Generac Next Generation Series (10–28 kW) and Guardian Series (2017–present, 10–26 kW) air-cooled home standby units. Where to view run hours: Mobile Link app/website (and Field Pro): available for all supported models; required for Next Generation Series. Generator control panel (Guardian only): ESC → SUB MENUS → MAINT → Run Hrs; then return to AUTO (“Ready to Run”). If you have high run hours or the warranty is ending: Check warranty status in Mobile Link. Consider purchasing an extended warranty through a Generac dealer. Follow the maintenance schedule to keep the unit in optimal condition. Troubleshooting tip: If you can’t navigate the control panel menus, see the linked control-panel article.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support