How to Determine If an Extender is Compatible with Mobile Link Wi-Fi

This article explains how to determine if a Wi-Fi extender is compatible with Mobile Link Wi-Fi for Generac home standby generators. Mobile Link requires a stable 2.4 GHz connection using 802.11b/g/n protocols, and dual-band or 5 GHz networks are not supported. Customers searching for “Mobile Link Wi-Fi compatibility,” “generator weak Wi-Fi signal,” or “generator won’t connect to Wi-Fi” will learn how to verify extender specifications, ensure a dedicated SSID, and maintain reliable connectivity. Following these steps improves signal strength, stable generator monitoring, and overall performance for generators with onboard Wi-Fi or Wi-Fi/Ethernet devices.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support