Is my Wi-Fi network compatible with Mobile Link's Onboard Wi-Fi Module?

This article explains Wi-Fi compatibility for Generac home standby generators using Mobile Link. Generators with onboard Wi-Fi or Wi-Fi/Ethernet devices must connect to a dedicated 2.4 GHz network, since 5 GHz is not supported. Customers searching for “generator Wi-Fi compatibility,” “generator won’t connect to Wi-Fi,” or “weak Wi-Fi signal generator” will learn how to split dual-band routers, avoid band steering, and confirm network requirements. These steps improve signal strength and connection stability, ensuring reliable generator monitoring and performance.

Title
Is my Wi-Fi network compatible with Mobile Link's Onboard Wi-Fi Module?
URL Name
Is-My-Wi-Fi-Network-Compatible-With-Mobile-Link

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support