Connect a generator to a home Wi-Fi network using a web browser (legacy method)

Learn how to connect a Generac Guardian home standby generator with Mobile Link Onboard Wi-Fi, not the aftermarket Wi-Fi/Ethernet device or cellular accessory, to a 2.4 GHz network using a web browser when the Mobile Link app setup fails or the generator won’t connect to Wi-Fi. The steps show how to join the MLG network, open 192.168.51.1 on iPhone, Android, or Windows, and handle captive portal or “no internet” prompts. Check signal strength if you have a weak Wi-Fi signal generator, then return the unit to Auto for stable monitoring and reliable operation.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support