What's are the differences between air and liquid-cooled generators?

Air-cooled generators come with engines that use fans to force air across the engine for cooling, while liquid-cooled generators use enclosed radiator systems for cooling, similar to an automobile. Generally, liquid-cooled engines are used on larger kW generators due to the larger engines required for the higher power output.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support