What Fuel Type Do Home Standby Generators Run On?

Home standby generators typically run on **liquid propane (LP)** or **pipeline natural gas (NG)**, depending on the model. Many Generac **7 kW–48 kW** units ship set up for **NG** and can be **converted to LP** in the field; some **60 kW and 80 kW (4.5 L engine)** models can also be converted. Diesel standby models (e.g., RD series) use **ULSD (S15)** and are more common in commercial applications. Fuel supply and installation requirements vary (propane tank size, gas meter capacity, regulators, pressure, pipe sizing); always confirm in the owner’s/installation manual and follow local codes. Users searching for "standby generator fuel conversion" will find answers here.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support