What Is CO-Sense™ Technology?

CO-Sense™ technology offers robust protection against hazardous levels of carbon monoxide that are present in engine exhaust. The technology employs advanced sensor technology that detects elevated CO levels quicker than standard household detectors. If high CO levels are detected, the generator engine is automatically shut off, and the user is alerted with a flashing red LED. 

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support