What Is an Integrated Smart Air Conditioning Module (SACM)?

The Integrated Smart Air Conditioning Module (SACM) is a built-in load management device available in select automatic transfer switches (ATS) that helps prevent generator overload during standby operation. It manages up to four air conditioning loads by automatically shedding and restoring them based on generator frequency and system demand. When the generator is running, the SACM temporarily disables all connected HVAC loads and then re-enables them in priority order using timed intervals. If an overload condition is detected, loads are shed and the affected priority is locked out for 30 minutes before the system attempts to restore it again. The module monitors generator frequency to determine overload conditions and uses status LEDs to indicate load activity.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support