What Is the Maximum Pressure That Should Be Supplied to the Generator’s Demand Regulator?

The maximum pressure that should be supplied will be dependent on the supplied fuel type. For natural gas units, the required fuel pressure for current products is 3.5-7" WC (.13-.25 PSI). For liquid propane vapor units, the required fuel pressure for current Evolution products is 10-12" WC (.36-.43 PSI). Pressure that is too high or too low can cause the engine to not start, run rough, be unable to support a load, and in some cases cause premature engine failure.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support