What type of oil should I use in my home backup generator?
This article provides guidance on the oil requirements and maintenance tasks for Generac air-cooled home standby generators. Generac recommends the use of 5W-20 full synthetic oil for all home standby generators, but owners can also use SAE 30, 10W-30, or 5W-30 synthetic oil. Oil changes are necessary for the generator engine and this must be performed according to the generator's maintenance schedule as described in the owner's manual. The first oil and oil filter change should be done when the generator reaches the end of its break-in period, which is defined as the first 25 hours of use.