What is a Power Management Module (PMM)?
The Power Management Modules (PMMs) is a 50A, 24VAC rated contactor. Through the use of PMMs, up to 4 large electrical loads can be managed when used in conjunction with some 100-800A, single-phase switches utilizing an Overload Prevention Control Board (OPCB). This allows for the use of a smaller, more affordable generator system.