What is a Generac Load Manager (previously known as a Smart Management Module (SMM))?
The Generac Load Manager formerly known as Smart Management Module (SMM) is a control wire-free device used to manage large electrical loads and prevent overloading during generator startup. It can manage up to 8 loads and is self-aware, with a built-in circuit board that monitors frequency, and can be used with 4 SACM loads for a total of 12 managed loads. The SACM can manage 2 ACs and four larger loads older technology. The New Intergrated SACM can manage 4 ACs.