Why Can’t I Connect My Generator to Wi-Fi With an Eero?
Mobile Link Wi-Fi connects only on 2.4 GHz. Eero’s mesh/band steering can push devices to 5 GHz, preventing setup or causing drops. Verify your network meets Mobile Link Wi-Fi requirements. During setup, temporarily hide/disable 5 GHz in the Eero app so the generator joins 2.4 GHz, then restore normal settings. If connectivity issues continue—or if your generator isn’t Wi-Fi compatible—consider the Connectivity Cellular Accessory, which uses multiple carriers for broader coverage and reliable monitoring.