Why Can't I Connect My Mobile Link-Enabled Generator to A 5.0 Ghz Wi-Fi Network?

This article explains why Generac Mobile Link Wi-Fi devices require a 2.4 GHz network instead of 5 GHz, how to split a combined network SSID for better connectivity, and when to consider adding a dedicated 2.4 GHz Wi-Fi extender or upgrading to the Generac Connectivity Cellular Accessory for improved generator monitoring and remote access.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support