Salesforce

Generac Load Manager Troubleshooting Guide

« Go Back
Fields
Generac Load Manager Troubleshooting Guide
Generac-Load-Manager-Troubleshooting-Guide
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns. 

Generac Load Manager troubleshooting guide

This article provides a troubleshooting flowchart for basic operational issues with Generac Load Managers.
 

Environment 

This article applies to 50A and 100A Generac Load Managers. 

Note: Previous versions of the Load Manager were formerly known as Smart Management Modules (SMM).

 

Generac Load Manager troubleshooting flow chart 

Load Manager SMM smart management module troubleshooting diagram   

The flowchart above can also be found in the owner's manual. To locate a copy of the owner's manual for the load manager, enter the serial number or model number on the Generac.com product information page.

If unable to resolve the issue using the steps provided above, it may be necessary to contact a Generac authorized service dealer.

Additional resources 

 
 

Powered by