Salesforce

How long will my home standby generator run?

« Go Back
Fields
How long will my home standby generator run?
How-long-will-my-home-standby-generator-run
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns. 

 

Factors influencing generator run time

Air-cooled home standby generators are designed to run for extended periods during power outages, requiring a shutdown and inspection after every 24 hours of continuous run time. Having a sufficient natural gas or propane fuel supply allows permanently installed home standby generators to run for longer periods of time than portable generators. 

 

That said, during extended outage scenarios, the maintenance schedule outlined in the owner's manual should be followed. This includes required shutdown and inspection every 24 hours. To keep track of run hours, see: How do I find out how many run hours are on my home standby generator?

 

 

The below links summarize the most important tasks and considerations when preparing to run a home standby generator continuously during extended outage scenarios.

 

Environment

This article applies to Generac air-cooled standby generators that are approaching or exceeding 24 hours of continuous use. The links below provide guidance on the most important maintenance tasks to consider in these scenarios.

Maintenance

After every 24 hours of continuous operation, it is crucial to safely shut down your home standby generator so that it can cool down and a series of operational checks to be performed. Before any maintenance can be completed, the generator must be safely removed from the home's electrical load and shut down appropriately.

  1. How Do I Shut Down My Generator When It’s Powering My House (During an Outage)?
  2. Continuous use maintenance for home standby generators

If needed, reach out to a service dealer in your area: How Can I Find a Generac Service Dealer in My Area?

 

Fuel & oil levels

Fuel supply and oil levels are crucial factors that influence a generator's performance and run time.

 

Additional considerations

 

 


Powered by