Continuous use maintenance for home standby generators

This article explains continuous use maintenance for Generac Next Generation Series 10–28 kW and Guardian Series 10–26 kW air-cooled home standby generators running for 24 hours or longer. It covers safe shutdown, oil checks, leak inspections, maintenance intervals at 25, 100, 200, and 400 hours, extreme-temperature requirements, and post-maintenance steps. Following these guidelines helps support safe operation, reliable performance, and extended generator lifespan.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support