What Does It Mean When My Generator Displays an Error Code: Charger Missing AC, Code 2780?
Explains Charger Missing AC code 2780, the T1 charging circuit conditions that can trigger it, and troubleshooting for Guardian and Next Generation home standby generators. It also explains when some Next Generation generators may continue showing the warning even though the battery is charging normally and when an IASD should perform further diagnosis.