Salesforce

Why did I get a "limit reached" error in Mobile Link?

« Go Back
Fields
Why did I get a "limit reached" error in Mobile Link?
Why-did-I-get-a-limit-reached-error-in-Mobile-Link
Content

Limit Reached message in Mobile Link

This error indicates that the maximum devices of that type for the account have been reached. As of Mobile Link version 3.8, device limits are: 

  • 2x Home Standby Generator
  • 4x Fuel monitoring devices

What can I do if I need to add additional generators?

At this time, the only way to add additional devices beyond the above stated limits is to enroll in a dealer-managed plan: How do I upgrade to a Dealer-Managed plan in Mobile Link?

If you need to remove a generator from your account here are instructions to do so. If you need assistance with removing a generator from your account, contact customer support: How Do I Contact Generac Customer Support?

 


Powered by