Battery voltage is very low fault (2751)

The “Battery Voltage is Very Low (2751)” fault occurs when the generator’s battery charge falls below 9 VDC for over 60 seconds. Found on Next Generation Series air-cooled home standby generators with the Power Zone 200 control panel, this warning may also appear as a battery fault, low voltage alarm, battery charging issue, or charger warning on new installation. Check battery cables, terminals, and charger wiring, then allow up to 18 hours for charging. If the alert persists, replace the battery or contact a Generac dealer.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support