Controller displays No/Bad SSID at the end of the connection process

The "No/Bad SSID" error occurs during the Wi-Fi connection process on a generator with a Mobile Link Wi-Fi device. This issue is typically caused by a provisioning problem with the router, which struggles to complete the setup. To troubleshoot, power cycle the router by unplugging it for 1-2 minutes, then wait up to 10 minutes for it to reconnect before trying the connection process again.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support