Mobile Link device historyMobile Link has been around since 2013/2014-time frame starting with the CDMA cellular deviceJul 3, 2025Knowledge
FieldsTitleMobile Link device historyURL NameHistory-of-Mobile-Link-DevicesContentPublic AnswerMobile Link device history A connectivity device refers to the hardware module containing the antenna and components that allow communicating generator controller data wirelessly to Mobile Link. This article provides historical context for each of these devices. To see compatibility information for each device and generator controller, see: Mobile Link Wi-Fi, Cellular, and LTE device compatibility guide Current devices Connectivity Cellular Accessory: Standard connectivity device included in newer model generators, also can be purchased as an after-market upgrade (see below)Released February/March 2025Part number G0072150Uses towers across carriers via dual sim cards Details on Carrier and More Upgrade compatibility: Compatible with all generator controllers that were compatible with the Onboard Wi-Fi, 4G/LTE, and Wi-Fi/Ethernet devices See here to upgrade: Connectivity Cellular Accessory Onboard W-Fi Device: Installed in the factory for Guardian series generators (not an aftermarket device)*Released on generators June/July 2018Part number (original A0000538695) A0002197676 Uses the home Wi-Fi network at the installation site of the generator *During a manufacturing shortage, there was a campaign to provide this device as an aftermarket accessory to new generator owners as they became available: Is the Wi-Fi Kit Compatible with My Generator? Legacy Devices These devices have been replaced by the above Connectivity Cellular Device. Connectivity products designated as "accessory devices" were available as aftermarket devices that could be retrofit to a compatible generator. This allowed generator owners to connect their units to Mobile Link, even if the generator did not originally ship from the factory with a connectivity device. CDMA Device: Released in approximately 2013/2014 Discontinued and no longer usable due to CDMA network being shut downPart number G0064630This device was a cellular 1x/2G deviceUsed Verizon Towers (Support for this device and the compatible Verizon Towers was discontinued on December 31, 2022) 4G LTE Accessory Device: Aftermarket accessoryReleased April 16, 2019Discontinued, but still being used in many unitsPart numbers: The original Part for Full kit G0071690 was discontinued on May 26, 2023Retrofit (discontinued) G00702020 was utilized as a CDMA upgradeUpdated Part: G0072080 May 26, 2023- current Can no longer be purchased (retailers or dealers may still have some) but can still be used Uses Verizon Towers Wi-Fi/Ethernet Accessory Device: Aftermarket accessoryRequires a dedicated 2.4 Ghz wireless network: Is My Wi-Fi Network Compatible With Mobile Link?Released June 2020Discontinued, but still being used in many unitsPart Number G0071700Became standard on liquid-cooled generators starting in approximately November 2021Used the home network at the installation site of the generator
Was this article helpful?Choose a general reason-- Choose a general reason --FeedbackUpload FilesUpload FilesOr drop filesSubmit