How do I find my generator's Wi-Fi SSID or "'MLG" network name?

To access the SSID from the generator control panel, press OFF, then Select WIFI and scroll until SETUP SSID: MLGXXXXX is displayed. If utilizing an accessory Wi-Fi/Ethernet device this will be located on the back of the device (or on your phone during connection)

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support