Connecting the Wi-Fi/Ethernet Mobile Link device to your home network

The Mobile Link™ Wi-Fi/Ethernet accessory allows generator owners to connect their devices to a home network either wirelessly or via a wired Ethernet connection, but only one method can be used at a time. Users must have certain items ready, such as an Ethernet cable (if using a wired connection), Wi-Fi credentials, and enclosure keys to access the generator. The connection process involves using the Mobile Link for Generators app to enable the accessory and configure it for either Wi-Fi or Ethernet, following specific setup steps depending on the chosen method.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support