How long will my load be locked out if it causes an overload when using a SACM or Load Manager?

When a Generac Load Manager or Integrated Smart Air Conditioning Module (SACM) enables a managed load that overloads the generator within 15 seconds, that load is locked out for 30 minutes, then reattempted. There’s no permanent lockout; the timer resets when utility power returns or the generator is shut down. If an AC won’t start, avoid changing load manager settings and contact a dealer—this guidance applies to transfer switches with a SACM or load manager—so managed loads operate safely and reliably (search: “SACM lockout time,” “load manager lockout,” “AC not coming on”).

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support