How to install a breather warmer?

This article provides step-by-step instructions for installing a breather warmer or breather heater component of the Generac cold weather kit for use in extreme cold weather applications where heavy icing occurs (0 °F or 18°C and below) on specific Generac air-cooled generators manufactured after 2013. It also includes procedures for preventing accidental generator startup and completing the installation process, including information on verifying proper oil type and quantity.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support