Mobile Link Wi-Fi keeps disconnecting

PowerCHAT Jun 19, 2024, 11:48:01 AM The generator may fail to maintain a stable Wi-Fi connection with your home network due to various reasons such as an internet outage, the number of devices connected, change in signal blockers, and insufficient bandwidth. If the issue persists, you should contact your ISP as they can identify certain causes and help with the problem. Mobile Link checks in with the router and internet service every 15 minutes, and if no response is received for three hours, it switches from online to offline status.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support