Troubleshooting guide for home standby Generators during an outage

Troubleshooting steps for air-cooled home standby generators during a utility outage, including: generator won’t start, or the generator is running but the home has no power (no power, not supplying power, running but no electricity, generator on but house/off, gen is running i dont have power, outlets dead, not transferring, transfer switch/ATS not switching, breaker/MLCB off), plus yellow/red light alarms, running continuously for 24+ hours, or continuing to run after utility power returns. Homeowners should only perform these steps if comfortable and should contact a Generac Service Dealer whenever possible; additional support resources (dealer locator and Customer Support) are included.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support