What Type of Oil Is Recommended for Use With Generac Portable Generators?

Above 32°F, use SAE 30. Below 40°F and down to -10°F, use 10W-30. Synthetic 5W-30 can be used in all temperatures.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support