What does “Wi-Fi not configured” mean in Mobile Link for the Connectivity Cellular Accessory?

Mobile Link may show “Wi-Fi not configured for your cellular connectivity accessory” when the optional Wi-Fi backup feature on the Connectivity Cellular Accessory is not set up. Cellular connectivity can still work without Wi-Fi configured, and Wi-Fi is only used as a fallback if cellular is unavailable. Use the linked steps to configure Wi-Fi backup for a more resilient connection and fewer connectivity interruptions.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support