What is the maximum distance a standby generator can be installed from a house or building?

Explains that there is no single maximum distance requirement for placing a Generac home standby generator from the house it powers. Distances (such as 110 feet) may be acceptable when wiring is properly sized, minimum clearance requirements are met, and the installation complies with local codes. Highlights key design considerations for longer runs (power conductors, applicable control wiring limits, and fuel supply). Includes links to clearance guidance, NFPA 37 info, where to find installation manuals, the product lookup page, and the dealer locator for help designing the installation correctly.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support