Why Is My Pump Experiencing Low/No Suction or Weak Discharge?

To troubleshoot low/no pump suction or weak discharge, check if the vertical suction lift and total head lift are within the allowed range, if the pump has been primed, if the end of the suction hose is submerged in water and suction hose strainer is obstructed, if suction hose or port is leaking air or water, if discharge hose or port is leaking air or water or if the discharge hose is blocked or restricted. Lastly, check the engine throttle lever and make sure it is set to the fast position.

Title
Why Is My Pump Experiencing Low/No Suction or Weak Discharge?
URL Name
Why-Is-My-Pump-Experienceing-Low-No-Suction-or-Weak-Discharge

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support