Will An Automatic Transfer Switch Continue to Draw Current When the Generator Is Not Running?

This article explains the normal power present at a Generac automatic transfer switch (ATS). It clarifies that the ATS has constant 240 VAC supplied by two 120 VAC lines, and that it also draws a small amount of 120 VAC on the T1 circuit for battery charging. Use this information when troubleshooting questions like “ATS has power,” “T1 circuit voltage,” “charger missing AC,” or low battery concerns, helping ensure reliable starting and operation.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support