Will Mobile Link WIFI devices work with Starlink internet?
Just like any internet service out there, it is dependent on the signal you are getting at the location you are trying to connect at as well as the frequency (2.4 GHz versus 5 GHz) (Most IoT devices can only connect to a 2.4 GHz network)