Salesforce

Home Standby Generator Engine Cranks But Will Not Start, or Starts Hard and Runs Rough

« Go Back
Fields
Home Standby Generator Engine Cranks But Will Not Start, or Starts Hard and Runs Rough
Home-Standby-Generator-Engine-Cranks-but-Will-Not-Start-or-Starts-Hard-and-Runs-Rough
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns.

Engine cranks but will not start or runs rough

This article covers the most common issues but is not exhaustive. If these steps do not identify or resolve the issue, generator owners should reach out to a local authorized service dealer. See the How Can I Find a Generac Service Dealer in My Area? article for more information.

Environment

This article applies to:
  • Generac Next Generation Series 10-28 kW air-cooled standby generators
  • Generac Guardian Series 10-26 kW air-cooled generators (2017 to present)

Troubleshooting

1. Check Mobile Link or the generator control panel for error codes

  • When a generator isn't working properly, the issue is often indicated by an error code. Depending on the generator model, error codes are visible in different places:

2. Was the unit recently installed?

Note: These steps should be performed by an IASD.

  • Ensure fuel is turned on. A shutoff valve should be within 6 feet of the unit.
  • Verify fuel lines have been bled. Air pockets in the line will prevent the unit from starting. This is especially common if LP was recently refilled.
  • Check for an empty or low LP tank.
  • Verify proper fuel conversion if running on LP.

3. Is this an existing install? When was maintenance last completed?

To schedule an inspection or service call, contact your local Generac authorized service dealer. See the Where Can I Find a Generac Dealer in the U.S. Or Canada? article for more information.


Powered by