Salesforce

How do I prepare my portable generator for a storm?

« Go Back
Fields
How do I prepare my portable generator for a storm?
How-do-I-prepare-my-portable-generator-for-a-storm
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns. 

Preparing and managing your portable generator during a storm

As a storm season approaches, ensuring that your portable generator is ready can be a lifesaver. Portable generators provide crucial backup power during outages but require careful handling to ensure safety and efficiency. This article guides you through preparing, operating, and safely managing your portable generator during a storm. 

Environment

  • Portable generators: This article applies to general portable generators 
  • Storm preparedness: This article is for portable generator owners who may need to prepare for storm-related outage. 
     

Preparation before the storm

1.Download a copy of your portable generator's user manual: Where can I download a user manual for my Generac portable generator?

Internet and cellular connection is not guaranteed during a severe outage. Download a local copy of your user manual that can be accessed offline. 

2. Check and charge the battery (if applicable): Ensure the generator's starter battery is fully charged. A well-charged battery is essential for starting the generator, especially in cold weather. Portable generator battery charging guidelines vary by model. To review specific charging guidelines for your portable device, see your owner's manual: Where can I download a user manual for my Generac portable generator?

3. Perform a test run: Conduct a test run to ensure the generator operates smoothly, and check for any unusual noises or vibrations. See our portable troubleshooting guide for help addressing any issues here: Portable generator troubleshooting guide

4. Inspect and perform any required maintenance: Regularly inspect the generator for any wear and tear.

5. Fuel supply: Have an adequate supply of fresh fuel stored in a safe location.

  • Use approved fuel containers to avoid moisture contamination.
  • Use a fuel stabilizer. 

6. Run the generator in a safe location: Set up the generator a minimum of 20 feet from any doors, windows, vents, or other openings into the home.

7. Review your user manual for safe start up and operation: Where can I download a user manual for my Generac portable generator?

Starting operation 

  1. Ensure safety first - Before starting the generator, double-check that it is placed in a well-ventilated area to avoid carbon monoxide buildup. 
  2. Verify that the engine oil level is correct.
  3. Verify fuel level is correct.
  4. Verify that the unit is secure on level ground. 

Note: The steps for starting up the generator may vary by model. See the owner's manual for model-specific operational steps here Where can I download a user manual for my Generac portable generator? 

8. Inspect extension cords for damage: Never use frayed or defective extension cords, as they may cause electrocution. Always be sure the extension cord is sized appropriately for the appliance: Power Cords vs. Extension Cords: How to select the right power cord and extension cord for your portable generator

Operating the generator during a storm

IMPORTANT: Operating a generator in wet conditions can be extremely hazardous and is strongly advised against. Never run a generator directly in the rain, snow, or any other wet conditions.

For carbon monoxide (CO) safety, always operate the generator outdoors in an open area. Never use it inside homes, garages, or enclosed spaces. 

1. Monitor operation: Never allow the unit to run out of fuel while supporting a load. Doing so can damage the unit and/or any connected loads. 

  • Regularly check the generators for warning signs 
  • Keep the generator dry and out of the rain. 

2. Observe safe practices with electricity:

3. Perform periodic shutdowns as specified in your owner's manual:

  • Every 8 hours, the portable generator must be shut down for a minimum of 30 minutes.  
  • During prolonged, continuous operation, the generator must be shut down to perform maintenance checks and refuel.

4. Follow safe refueling practices:

  • Always shut down the generator before refueling.
  • Always disconnect any loads from the generator before shutting it down. 

5. Follow safe engine shutdown practices:

1. Important: Remove all loads from the generator before shutting down. See: Do I need to remove loads before shutting down my portable generator? 
2. Cool Down - Allow generator to run without a load for a few minutes to stabilize internal temperatures before shutting down. 
3. Place the generator in the OFF position. 
4. Turn the generator fuel valve OFF (if equipped).
 


Powered by