What does it mean when my generator displays an alarm: Overload Remove Load, error codes 2100-2103

Error codes 2100-2103, labeled as "OVERLOAD REMOVE LOAD," indicate an overload condition in Generac air-cooled home standby generators. Troubleshooting involves identifying and removing non-essential loads, checking load management devices for proper functionality, and clearing the alarm from the control panel. To prevent future overload alarms, users should regularly assess load capacity, ensure proper load management configurations, and follow routine maintenance schedules.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support