Generac Home Standby Error Codes: Red/Yellow Light Meanings, Mobile Link Messages & Fixes

This article helps you look up Generac home standby generator error codes (also called alarm or warning codes), what the red and yellow lights mean, and the Mobile Link message you’ll see in the app. It lists the most-searched codes—1100 Overcrank, 1200 Overspeed, 1300 Low Oil Pressure, 1400 High Temperature, 1500 RPM Sense Loss, 1600 Underspeed, 1900 Undervoltage, 2098–2099 Wiring Error, 2100 Overload/Remove Load, 2400 Fuse Problem, 2750 Low Battery, 2770 Charger Warning, 2780 Charger Missing AC, 2800 Auxiliary Shutdown, 1063, and Error Code 0—and links to step-by-step articles. Use it to confirm whether your status is an Alarm (red) or Warning (yellow), see the corresponding Mobile Link message, and jump to fixes. Works for Evolution controllers (on-screen + app) and Power Zone 200 (app only). Includes how to clear an alarm, perform a hard reset, and when to contact a Generac dealer for service.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support