What Does It Mean When My Generator Displays an Alarm: Underspeed, Error Codes 1600-1603
Error codes 1600-1603, labeled as "UNDERSPEED," indicated an issue with engine speed potentially due to overload condition, fuel system, or lack of routine maintenance. Troubleshooting involves basic checks of these components and clearing the alarm from the control panel. Context of the scenario when the error appears may provide additional insights to the issue. This article also provides next steps after troubleshooting, and working with a Generac IASD.