How do I verify the correct fuel selection is selected for my generator?

This article explains how to confirm that a Generac home standby generator is set to the correct fuel type. It outlines how to verify the mechanical fuel valve position on Guardian-series units, check the fuel selection setting in the Evolution control panel, and understand fuel configuration requirements for the 7.5 kW PowerPact model. It also notes that Next Generation units use the Field Pro app for fuel setup. This helps ensure proper operation, reliable starting, and safe performance.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support